MII Connection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MII Connection problem

4,235件の閲覧回数
alessandromaggi
Contributor I

Hi,

I have a custom board(designed by us) based on IMX6 SoloX. This board has (among other) two optical ports 100-FX, realized connecting a micrel KSZ8873FLLI via MII to the SoloX.

The problem is that I found an unexpected electrical level on the MII interface in TX direction. I would like the high level to be 3.3V, but on the oscilloscope I quite often can see a stable level around 2 volts.

So on the TX line I can see 3 different voltage level: 3.3V (expected igh level), 2V (unexpected and unwanted high level), and 0V (low level).

Of course with this condition the port is not working.

My question are:

1) Is it possibile for the SoloX to work with an MII interface with 3.3V as high level ? The reference manual is not very clear on this topic.

2) If yes, how the NVCC_SGMII should be connected ?

3) What can cause this strange 3 level signal ?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

4,040件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  Alessandro

one can recheck enet power supplies connections using

i.MX6SX Datasheet Table 110. 19x19 mm Functional Contact Assignments

"Power Group" column
https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Also one can look for layout errors and short circuit between traces.

3.3V is allowable value according to Table 10. Operating Ranges i.MX6SX Datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信