IMX6UL frame buffer question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL frame buffer question

3,553 Views
anshulkhare
Contributor III

Hi,

My platform is i.mx6ul, i have enabled the frame buffer driver in menu configuration.but it is not visible in

/dev file system

If I look at /sys/class/graphics on my card, I am not able to find frame buffer

 Could any one help me to solve this issue?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

3,267 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

please refer to sect.12.3 Software Operation attached Linux Manual

for description of frame buffer for i.MX6UL.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply