MFGtool MultiPanel is not loading the uboot properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGtool MultiPanel is not loading the uboot properly

2,086 Views
dibing
Contributor I

Hi,

we have designed a Vehicle Automotive system with using NXP iMX6Q processor in Sabre platform. We are using eMMC and SD card as boot devices.

Here we are using MFGtool for ubooting the cpu and this is the first time with MFGtool

we have selected the "mfgtool2-android-mx6dqscm-1gb-qwks-rev2-sd.vbs" and started the ubooting after connecting the USB otg port of our board to USB port of HOST computer.

But, after loading kernal the MFGtool Multipanel is showing "Loading U-boot" and no further changes in the screen. There is no console in UART also. 

But we are getting console in the Linux system using Usb loader.

How can I solve the problem with MFGTOOL ??

** I have attached the MfgTool_MultiPanel window here

Tags (1)
0 Kudos
Reply
1 Reply

1,819 Views
jimmychan
NXP TechSupport
NXP TechSupport

please make sure you are selecting the proper vbs file that match your board.

the main script of mfgtool is ucl2.xml. Basically, the vbs file + cfg.ini are used to setup the variables in the script. You can modify the script content directly to match your board and the filename of images. Please let me know if you have any question about the script.

0 Kudos
Reply