Hi,
We have to flash our custom image (Bootmanager, Integrity monolithic [kernel+VAS]) to NOR/NAND flash using MFG Tool using Serial Download mode.
Currently NOR and NAND has 4 partitions. The Bootstrap kernel and U-Boot is partitioning the NOR and NAND chip.
Is there any way to change this partition size?
Or we have to create new Bootstrap U-Boot and kernel image with new partition configuration?
Regards,
Karthikeyan,
+919043955880
Hi Karthikeyan
seems partitions are defined in dts file, like
Linux/arch/arm/boot/dts/imx53-evk.dts - Linux Cross Reference - Free Electrons
can be changed in kernel boot parameters as described in attached Linux Guide
sect.4.6 Flash memory maps.
For mfg tools partition operations one can look at attached ucl2.xml
from mfg-tools 3.14.28_1.0.0 release
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ,
Thank for your reply. I have number of questions.
1. Which build system Freescale used ? Yocto or LTIB?
2. We are using i.MX_6_Linux_Reference_Manual.pdf guide to create the kernel image. It is mentioned in
Chapter 43
EIM NOR Driver
arch/arm/mach-mx6/board-mx6q_sabreauto.c file the NOR partition is done.
But i am not able to find this file in Freescale git as well as Yocto community git.
linux-2.6-imx.git - Freescale i.MX Linux Tree
Which git repositary or any patch to be added or guide to refer for kernel and uboot image creation.
3. In Manufacturing Tool V2 Linux or Android Firmware Development Guide V2.docx Page no:3 mentioned that
Please refer to the BSP User Guide, chapter Build Manufacturing Firmware 
Which BSP user guide its mentioned?
4. We need two u-boot (1. In bootstrap mode 2. Actual which will be flashed.)
In Freescale_Yocto_Project_User's_Guide.pdf 6.2 The Manufacturing Tool, MFGTool mentioned that u-boot-mfgtool recipe in Yocto used to create uboot image for MFGTool.
Is is the image used in Bootstrap mode or actual image to be flashed.
Our goal is to create the Bootstrap mode U boot and kernel image with our own partition layout. Please help us.
Regards,
Karthikeyan,
+919043955880
1. as you did not specify, answer was provided for default, latest L3.14.28
2. one can look at
Linux/Documentation/devicetree/bindings/bus/imx-weim.txt - Linux Cross Reference - Free Electrons
3. "BSP User Guide, chapter Build Manufacturing Firmware " in L3.14.28 Linux BSP means
sect.6.2 Manufacturing Tool, MFGTool Freescale_Yocto_Project_User's_Guide.pdf,
attached, also can be found on
Supporting Information (14)
L3.14.28_1.0.0_LINUX_DOCS (REV L3.14.28_1.0.0)
i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
4. in 3.14.28 Mfg Tools folder /firmware contains files which are used by Mfg Tools
(firmware), folder /files - for flashing to media. It may be useful to look at ucl2.xml,
*.vbs files for better understanding.
~igor