Location of IOMUX Tool for i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Location of IOMUX Tool for i.MX6UL

ソリューションへジャンプ
5,626件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Where is a IOMUX Tool for i.MX6UL ?

I downloaded IOMUX Tool from following page but it wasn't included.

IOMUX Tool Introduction

Ko-hey

タグ(2)
0 件の賞賛
返信
1 解決策
3,255件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the Processor Expert instead.

For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.


An update has to be applied for the i. MX6UL.

http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,255件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Since SoloX the pin mux is support by Processor Expert for i.MX.

Processor Expert for i.MX|Freescale

Untitled.png

3,255件の閲覧回数
Danube
Contributor IV

Hi Sir,

Do you have i.MX6UL pin mux excel file ?

Process Expert can't copy all pin to excel file.

0 件の賞賛
返信
3,255件の閲覧回数
ko-hey
Senior Contributor II

Hi Yuri and Biyong

Thanks, I'll try it.

Ko-hey

0 件の賞賛
返信
3,256件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the Processor Expert instead.

For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.


An update has to be applied for the i. MX6UL.

http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,255件の閲覧回数
wowa
Contributor I

Hi All,

Hi Yuri,

i am not a software developer. I have no idea about eclipse.... So for me it is very difficult to use "Expert" instead of IOMUX Tool.

Does exist a "HowTo" for beginners or a easier way to check the pin configuration ?

I only want to see if my configuration with my wished functions is working or not.... In IOMUX you could see e.g.

in a diagram if you get a conflict or not....

Thanks for help beforehand.

0 件の賞賛
返信
3,255件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Basically You may manually check pin mux configuration, using section 4.1.1 (Muxing Options)

of the i.MX6UL RM.

Regards,

Yuri.

0 件の賞賛
返信
3,255件の閲覧回数
wowa
Contributor I

Hi,

but It is very complex with this method. I have solved the issue with PE right now.

If you are accustomed to work with IOmux tool the PE is a new world for HW-Developers.

Thanks.

Regards.

Wolfgang

0 件の賞賛
返信