MFG tool to read a file from imx28 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFG tool to read a file from imx28 

1,783 次查看
shashikanthirem
Contributor III

whats the command to read from the imx28 

i am using the following MFG tool version

pastedImage_1.png

i could able to dump the file from host PC to imx28 hardware, but not read from the hardware to PC

tried this to read file , 

<CMD state="Updater" type="pull" body="abc.sh" file="files/def.sh" timeout="60">copying shell script</CMD>

file got created def.sh in host , but some two bytes able read,

any one suggestion ?

2. this version MFG crash on windows 10 but not on win7

 

标签 (3)
标记 (2)
0 项奖励
回复
3 回复数

1,599 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The default BSP and released mfgtool for i.MX28 is support win7. So about on the win10 you can have a try the version MFG-Tool-V1.6.2.055.

0 项奖励
回复

1,599 次查看
shashikanthirem
Contributor III

Hi Rita,

i am using the same MFG-Tool still its failing

0 项奖励
回复

1,599 次查看
shashikanthirem
Contributor III

Still it's open...

0 项奖励
回复