MFG tool to read a file from imx28 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG tool to read a file from imx28 

1,823 Views
shashikanthirem
Contributor III

whats the command to read from the imx28 

i am using the following MFG tool version

pastedImage_1.png

i could able to dump the file from host PC to imx28 hardware, but not read from the hardware to PC

tried this to read file , 

<CMD state="Updater" type="pull" body="abc.sh" file="files/def.sh" timeout="60">copying shell script</CMD>

file got created def.sh in host , but some two bytes able read,

any one suggestion ?

2. this version MFG crash on windows 10 but not on win7

 

Labels (3)
Tags (2)
0 Kudos
Reply
3 Replies

1,639 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The default BSP and released mfgtool for i.MX28 is support win7. So about on the win10 you can have a try the version MFG-Tool-V1.6.2.055.

0 Kudos
Reply

1,639 Views
shashikanthirem
Contributor III

Hi Rita,

i am using the same MFG-Tool still its failing

0 Kudos
Reply

1,639 Views
shashikanthirem
Contributor III

Still it's open...

0 Kudos
Reply