MFG Tool Fails. Help..

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MFG Tool Fails. Help..

跳至解决方案
2,536 次查看
KeshavaGN
Contributor V

Hi all,

I'm trying to flash NAND using MFG tool. It fails frequently with following lines on hyperterminal :

PID:00400002 TID:01BF000E ERROR: c:\wince700\platform\common\src\soc\common_fsl_v3\uut\uutdrv\bot.cpp line 766: PID:00400002 TID:01BF000E UsbMsFn!BOT_HandleCBW: Invalid CBW signature

Error message on MFGTool displays:

failed to run command: type="push" body="send" file="files/NK.nb0" timeout="10" onError="" text="Sending NK.nb0 file." ,, Error code:-1

What is the reason for this error? and how i can solve it?

Thanks.

With regards,

Keshava G N


标签 (3)
0 项奖励
回复
1 解答
2,196 次查看
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,197 次查看
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

0 项奖励
回复
2,196 次查看
KeshavaGN
Contributor V