MFG Tool Fails. Help..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG Tool Fails. Help..

ソリューションへジャンプ
2,535件の閲覧回数
KeshavaGN
Contributor V

Hi all,

I'm trying to flash NAND using MFG tool. It fails frequently with following lines on hyperterminal :

PID:00400002 TID:01BF000E ERROR: c:\wince700\platform\common\src\soc\common_fsl_v3\uut\uutdrv\bot.cpp line 766: PID:00400002 TID:01BF000E UsbMsFn!BOT_HandleCBW: Invalid CBW signature

Error message on MFGTool displays:

failed to run command: type="push" body="send" file="files/NK.nb0" timeout="10" onError="" text="Sending NK.nb0 file." ,, Error code:-1

What is the reason for this error? and how i can solve it?

Thanks.

With regards,

Keshava G N


ラベル(3)
0 件の賞賛
返信
1 解決策
2,195件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,196件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

0 件の賞賛
返信
2,195件の閲覧回数
KeshavaGN
Contributor V