MDC frequency setting value and the actual measured value are difference between the two

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MDC frequency setting value and the actual measured value are difference between the two

1,776 次查看
charleshuang
Senior Contributor II

Internal MAC clock frequency value: 66 MHZ

PHY: Ar8031

1. After I set MDC frequency value(FEC_ENET_MII_CLK) are 1/2.36/2.5 MHZ in fec_enet_mii_init function, I measure the value is about 2.3/1.8/5.5 MHz.

    MDC frequency setting value and the actual measured value are big difference between the two.

    Can you please tell me how to set this value, the measured value will not differ too much?

2. I find that the formulas of reference manual and program are different.

   a) i.MX 6Solo/6DualLite Applications Processor Reference Manual (MII Speed Control Register):

       Internal MAC clock frequency / ((MSCR[MII_SPEED]+1)x2) = MDC frequency

       Example: 25 MHz / ((4 + 1) x 2) = 2.5 MHz

   b) Program (fec_enet_mii_init() in fec.c):

       fep->phy_speed = DIV_ROUND_UP(clk_get_rate(fep->mdc_clk),(FEC_ENET_MII_CLK << 2)) << 1;

       Can you please tell me which one is correct?

Thank you.

0 项奖励
回复
2 回复数

1,395 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Both formulas should be equivalent provided that the Linux formula should work as it’s the actual implementation of the driver. However, it’s sometimes possible that the code looks deceiving if you do not know where the variables are pointing to etc.

Would you please share the BSP version that you’re using and the location of the file? I’m having problems locating these lines on the latest BSP version. I also looked at the driver on the i.MX6 SDK and couldn't locate these lines.

0 项奖励
回复

1,395 次查看
charleshuang
Senior Contributor II

I use 3.0.35 BSP version. The location of the file is driver/net/fec.c. The function name is fec_enet_mii_init(struct platform_device *pdev).

Then you can see the following message in the program:

fep->phy_speed = DIV_ROUND_UP(clk_get_rate(fep->mdc_clk),(FEC_ENET_MII_CLK << 2)) << 1;

Example: Set MII speed to 1 MHz in program. However, the measurement results is 1.83 MHz.

0 项奖励
回复