Dear All,
I want to set frequency of MII clock(MDC pin).
I refer to the following point.
IMX6DQRM.pdf (Rev2)
- 23.5.7 MII Speed Control Register (ENET_MSCR) (P.1100)
- Table 23-12. Programming Examples for MSCR (P.1100)
Internal MAC clock frequency is listed in Table 23-12.
However, I do not know which this frequency shows.
Is this frequency set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn registers?
May I have advice?
Best Regards,
Yuuki
Solved! Go to Solution.
Hi yuuki
yes correct, internal MAC clock frequency is
set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki
yes correct, internal MAC clock frequency is
set in DIV_SELECT Field of CCM_ANALOG_PLL_ENETn register.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------