MCUXPresso IDE check Link application to RAM burn error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXPresso IDE check Link application to RAM burn error

1,612 Views
jarman_zhou
Contributor I

Hi,

I used MCUXPresso IDE to import a project evkmimxrt1020_iled_blinky, checked Link application to RAM, and compiled successfully. However, the following errors occurred when downloading to the EVK board, please help to analyze the problem,thanks.

20221024203805.png20221024203721.png20221024204215.png

0 Kudos
Reply
5 Replies

1,593 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

Since the application is link to SRAM, it needn't flash. But it seems you want to program it to flash. You method won't work.

To download SRA</SDRAM application to flash, lease refer to this post.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/I-MX-RT-How-to-booting-to-SDRAM/ta-p/1125054

 

Regards,

Jing

0 Kudos
Reply

1,589 Views
jarman_zhou
Contributor I

Hi.@jingpan,

Thank you for your reply!

I tried to operate it according to the link document you provided, but failed. The following are my steps and results.

1.Add DCD by MCUxpresso IDE

I completed steps 1-6 according to the article,Then use MCUBootUtility to download.s19 files to NOR flash,The following error message is displayed:

1.png

2.Add DCD by MCUBootUtility

In step 3, set the Device Configuration Data,I choose to C:\Users\Admin\Desktop\NXP-MCUBootUtility-master\src\targets\MIMXRT1021\evkmimxrt1020_xip_boot_header_dcd.bin,The following error is displayed when you click OK:

2.png

Regards,

jarman

0 Kudos
Reply

1,575 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

Where do you want the application run, SDRAM or DTC or OCRAM? All of them need to put the application at base_address+0x2000. Please try the second method again. I don't know why there is "permission denied" in your log. Is there security issue?

 

Regards

Jing

0 Kudos
Reply

1,573 Views
jarman_zhou
Contributor I

Hi,@jingpan

Thank you for your reply.

I put MCUBootUtility into another directory to successfully burn the application. I ran the application in SDRAM, but the program did not run after the burning, and there was no print out of the serial port. Here are my specific operation steps.

1.Memory configuration, specify RAM as SDRAM and modify the offset address.

1-1.png

2.Select Link application to RAM.

1-2.png

3.Compile the project and generate the.s19 file.

1-3.png

4.Configuration of DCD and burn the image.

1-4.png1-5.png

1-6.png

The above is my detailed operation steps.

When I tried to run in DTC, the LED was blinking but the debugging serial port still did not print.

Regards

Jarman

0 Kudos
Reply

1,565 Views
jarman_zhou
Contributor I

Hi,@jingpan

The problem has been solved, the reason is the IDE inside also want to add DCD macro, thanks.

Regards

Jarman

0 Kudos
Reply