MCLK clarifications with SAI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCLK clarifications with SAI

跳至解决方案
1,424 次查看
imx_user8
Contributor I

It isn't clear to me and I want to make sure I'm understanding the documentation correctly.

1. If we use the imx8m mini SAI as a slave then it is not necessary to use the imx8 MCLK, correct?

The documentation talks about using MCLK to generate the bit clock when master, but doesn't necessarily mention being used as a slave.

2. If we use the imx8m mini SAI5 as a master, it appears I can connect an external OSC to SAI2 MCLK and use that for SAI5.  Can I then output that same MCLK on the SAI5 MCLK pin?

标签 (1)
0 项奖励
回复
1 解答
1,387 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

1. Yes, that is correct.

2. Could you please share me a diagram of desired connection? Maybe you could use SAI5 as master to provide clock signals to SAI2 working as slave.

Best regards.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,358 次查看
imx_user8
Contributor I

Thank you.  I believe you've answered my questions as I can do the first option.  

0 项奖励
回复
1,125 次查看
zouhui
Contributor I

@imx_user8 

I am also suffering the clock configuration similar with your No.2 question, would you please share how to configure? Thanks

My application is that, SAI2 MCLK came from external IC, we want to reuse SAI2 MCLK for PDM clock. 

0 项奖励
回复
1,388 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

1. Yes, that is correct.

2. Could you please share me a diagram of desired connection? Maybe you could use SAI5 as master to provide clock signals to SAI2 working as slave.

Best regards.

0 项奖励
回复