MCLK clarifications with SAI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCLK clarifications with SAI

ソリューションへジャンプ
1,479件の閲覧回数
imx_user8
Contributor I

It isn't clear to me and I want to make sure I'm understanding the documentation correctly.

1. If we use the imx8m mini SAI as a slave then it is not necessary to use the imx8 MCLK, correct?

The documentation talks about using MCLK to generate the bit clock when master, but doesn't necessarily mention being used as a slave.

2. If we use the imx8m mini SAI5 as a master, it appears I can connect an external OSC to SAI2 MCLK and use that for SAI5.  Can I then output that same MCLK on the SAI5 MCLK pin?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,442件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

1. Yes, that is correct.

2. Could you please share me a diagram of desired connection? Maybe you could use SAI5 as master to provide clock signals to SAI2 working as slave.

Best regards.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,413件の閲覧回数
imx_user8
Contributor I

Thank you.  I believe you've answered my questions as I can do the first option.  

0 件の賞賛
返信
1,180件の閲覧回数
zouhui
Contributor I

@imx_user8 

I am also suffering the clock configuration similar with your No.2 question, would you please share how to configure? Thanks

My application is that, SAI2 MCLK came from external IC, we want to reuse SAI2 MCLK for PDM clock. 

0 件の賞賛
返信
1,443件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

1. Yes, that is correct.

2. Could you please share me a diagram of desired connection? Maybe you could use SAI5 as master to provide clock signals to SAI2 working as slave.

Best regards.

0 件の賞賛
返信