MCIMX8M-EVK HDMI setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCIMX8M-EVK HDMI setting

跳至解决方案
8,528 次查看
torus1000
Contributor V

Hi,

I downloaded linux demo image then wrote it to my sdcard.

demo image: https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_Beta
vcp-driver: https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers

$sudo dd if=fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard of=/dev/sdb bs=1M
$sudo dd if=imx-boot-imx8mqevk-sd.bin-flasg-hmdi-spl-uboot of=/dev/sdb bs=1k seek=33

It looked EVK boot up successfully but HDMI port output no signal at all.

How do I configure the display port for HDMI?

Once I tried to fix setenv of u-boot as following but nothing changed.

u-boot> setenv mmcroot /dev/mmcblk1p2 rootwait rw video=HDMI-A-1:1920x1080-32@60
u-boot> saveenv
u-boot> boot

Can anyone help me?

标记 (3)
1 解答
5,678 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Team,

The i.MX8M  has not officially release neither Android or Linux BSP,   so the support from NXP in the public community it is not available yet. Once the product has been release, we were able to discuss the features and functionalities of the device and the enablement tools, like Android and Linux.  To avoid any confusion at the moment the information it is subject to change without any notice.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
6 回复数
5,678 次查看
gabriel_h
Contributor V

It looks that Android image does support HDMI output out of the box

5,678 次查看
torus1000
Contributor V

Dear gabriel_h‌

According to your advice, finally I could see android demo following the "Android_Quick_Start_Guide.pdf".

document: https://www.nxp.com/docs/en/supporting-information/android_O8.0.0_1.3.0_8M-PRC_docs.tar.gz
mfgtool: https://www.nxp.com/webapp/Download?colCode=O8.0.0_1.3.0_ANDROID_TOOL_8MQ_BETA
android demo image: https://www.nxp.com/webapp/Download?colCode=O8.0.0_1.3.0_ANDROID_DEMO_8MQ_BETA

- Copied all images to the MFGTool-Dir/Profiles/Linux/OS Firmware/files/android/evk directory.
- In my case I used partition-table-7GB.img instead of partition-table.img.
- Double-clicked mfgtool2-android-mx8mq-evk-sd.vbs to write images to my 8GB SD card.
- After writing the images, boot the board.
- Set the U-Boot environment variables as follows:


 U-Boot > setenv bootcmd boota mmc0
 U-Boot > setenv bootargs console=ttymxc0,115200 earlycon=imxuart,0x30860000,115200 init=/
 init video=HDMI-A-1:1920x1080-32@60 androidboot.zygote=zygote64_32
 androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=800M
 androidboot.selinux=permissive
 U-Boot > saveenv
 U-Boot > boot

Now I know my problem caused by bad HDMI monitor which unofficially supported 1920x1080 size.
Actually I swapped to the another monitor it worked without any problems.

Sorry for bother you.

0 项奖励
回复
5,678 次查看
gabriel_h
Contributor V

Dear torus1000‌

You are not bothering me. We are here to help each other :smileyhappy:

You are welcome

0 项奖励
回复
5,679 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Team,

The i.MX8M  has not officially release neither Android or Linux BSP,   so the support from NXP in the public community it is not available yet. Once the product has been release, we were able to discuss the features and functionalities of the device and the enablement tools, like Android and Linux.  To avoid any confusion at the moment the information it is subject to change without any notice.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,678 次查看
gabriel_h
Contributor V

Dear jamesbone‌

According to this link

i.MX 8M Applications Processor | Arm Cortex-A53, Cortex-M4|NXP 

the i.MX8M is available for sale, and it seems like it has officially releases here

i.MX 8M Applications Processor | Arm Cortex-A53, Cortex-M4|NXP 

BR

Gabriel

0 项奖励
回复
5,678 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Torus,

Unfortunately the i.MX8M it is not release yet, so we do not have the tools to test and provide an answer. 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复