MCIMX6SLEVK Camera Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6SLEVK Camera Interface

1,483 Views
pankajrana
Contributor III

Hi,

Currently working with SoloLite EVK, I have few doubts on using the camera interface. The camera DOVDD is 1.8V.

All the signals coming to the "Camera Expansion Connector - J24" are EPDC signals, so if not using EPD, can we enable the LVE field (1.8V mode) for the camera related signals, including the EPDC_GDRL (CSI_MCLK)?

Or do we need to provide 3.15V to 1.8V level translators in an add-on board ?

Thanks.

Pankaj Rana

Labels (1)
0 Kudos
Reply
3 Replies

1,354 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

I think both solutions are possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,354 Views
pankajrana
Contributor III

Hi igorpadykov ,

CSI_MCLK.jpg

1. Since MCLK is provided by the CCM module directly, is it still possible to it in LVE mode ?

2. If it is possible to use configure LVE feature for Camera signals then we can directly wire up the Camera lines. Please confirm.

Regards,

Pankaj Rana

0 Kudos
Reply

1,354 Views
igorpadykov
NXP Employee
NXP Employee

1. this depends on pad (which is used for such purpose), if it has LVE setting,

then it is possible

2. yes

Best regards

igor

0 Kudos
Reply