MCIMX6Q-SDB Camera MIPI Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDB Camera MIPI Interface

Jump to solution
2,189 Views
louisryan
Contributor II

Hi,

I want to use the OV5640 camera.

I have a board MCIMX6Q-SDB but the MIPI connector J5 is missing from the board.

I can't modify the board as it is a on loan. I am happy to buy a new board.

Can this board be got with this connector and associated components populated?

What NXP supported development board would be suitable for this application?

Thanks,

Louis

Labels (1)
Tags (1)
1 Solution
1,996 Views
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,997 Views
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,996 Views
louisryan
Contributor II

Thanks Igor...

0 Kudos
Reply