How to interface freescale K81 with i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to interface freescale K81 with i.MX6?

1,465 Views
hrushinale
Contributor III

Hello Community,

For one of my application it requires to interface freescale K81 MCU with i.MX6 over SPI interface.

Do I need to write the driver for communication between these devices ?

If yes then please suggest some driver names for reference.

Thanks & Regards,

Hrushi

Labels (3)
0 Kudos
Reply
1 Reply

1,358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

one can try to adapt imx-test (folder /mxc_spi_test)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

just for reference one can also look at attached Linux Manual

Chapter 31 SPI NOR Flash Memory Technology Device (MTD) Driver

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply