MCIMX6Q-SDB Camera MIPI Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6Q-SDB Camera MIPI Interface

ソリューションへジャンプ
2,118件の閲覧回数
louisryan
Contributor II

Hi,

I want to use the OV5640 camera.

I have a board MCIMX6Q-SDB but the MIPI connector J5 is missing from the board.

I can't modify the board as it is a on loan. I am happy to buy a new board.

Can this board be got with this connector and associated components populated?

What NXP supported development board would be suitable for this application?

Thanks,

Louis

ラベル(1)
タグ(1)
1 解決策
1,925件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,926件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,925件の閲覧回数
louisryan
Contributor II

Thanks Igor...

0 件の賞賛
返信