MCIMX6Q-SDB Camera MIPI Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCIMX6Q-SDB Camera MIPI Interface

跳至解决方案
2,137 次查看
louisryan
Contributor II

Hi,

I want to use the OV5640 camera.

I have a board MCIMX6Q-SDB but the MIPI connector J5 is missing from the board.

I can't modify the board as it is a on loan. I am happy to buy a new board.

Can this board be got with this connector and associated components populated?

What NXP supported development board would be suitable for this application?

Thanks,

Louis

标签 (1)
标记 (1)
1 解答
1,944 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,945 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Louis

it is populated on Sabre SDP board

SABRE Platform for Smart Devices|NXP 

http://www.nxp.com/files/32bit/doc/fact_sheet/RDIMX6SABREPLATFS.pdf 

also one can check third party boards, like BD

https://boundarydevices.com/products/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,944 次查看
louisryan
Contributor II

Thanks Igor...

0 项奖励
回复