MCIMX6Q Migration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,215件の閲覧回数
PolarBear_88
Contributor II

Dear NXP

I have a question about wheather  two NRND devices(MCIMX6Q6AVT08AD, MCIMX6QP6AVT1AA) can be replaced by MCIMX6Q5EYM10AD.

When I reviewed to replace the above two devices to MCIMX6Q5EYM10AD, the only diffrences are Maximum frequency, SRAM and junction temperature.

Can I say to my customer that MCIMX6Q5EYM10AD is same in fuctionality as a alternative of MCIMX6Q6AVT08AD, MCIMX6QP6AVT1AA)

PolarBear_88_0-1691046508459.png

 

0 件の賞賛
返信
1 解決策
2,193件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

In hardware they are pin to pin compatible.

元の投稿で解決策を見る

1 返信
2,194件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

In hardware they are pin to pin compatible.