MCIMX6Q Migration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q Migration

Jump to solution
2,199 Views
PolarBear_88
Contributor II

Dear NXP

I have a question about wheather  two NRND devices(MCIMX6Q6AVT08AD, MCIMX6QP6AVT1AA) can be replaced by MCIMX6Q5EYM10AD.

When I reviewed to replace the above two devices to MCIMX6Q5EYM10AD, the only diffrences are Maximum frequency, SRAM and junction temperature.

Can I say to my customer that MCIMX6Q5EYM10AD is same in fuctionality as a alternative of MCIMX6Q6AVT08AD, MCIMX6QP6AVT1AA)

PolarBear_88_0-1691046508459.png

 

0 Kudos
Reply
1 Solution
2,177 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

In hardware they are pin to pin compatible.

View solution in original post

1 Reply
2,178 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

In hardware they are pin to pin compatible.