M4 gcc i686 host

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M4 gcc i686 host

1,790 次查看
davidpatton
Contributor III

Anyone know where I can get a pre-compiled GCC for the ARM M4 Cortex, hosted on i686-Linux? Everything I can find is for x86_64-Linux host. Thanks!

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,724 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can use the following:

GNU Toolchain | GNU-RM Downloads – Arm Developer  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,724 次查看
davidpatton
Contributor III

Thanks...but they only have the pre-built compiler for x86_64, not i686.

I hate the thought of it, but do you know if the source tarball is already configured to generate arm-none-eabi-gcc, et al?

0 项奖励
回复

1,724 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  You may try the following:

GNU Arm Embedded Toolchain project files : GNU Arm Embedded Toolchain 

Regards,

Yuri.

0 项奖励
回复