Arm PLL frequency configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arm PLL frequency configuration

2,483件の閲覧回数
n_po
Contributor I

Apologies if this has been asked previously.

There are 3 arm clock frequencies listed in the datasheet according to the part number:

Arm Cortex-A7 Frequency$$
528 MHz05
792 MHz08
900 MHz09

I would like to request for your expert opinion if there are consequences/issues (perhaps on the reliability of the arm execution, chip life) if I don't configure the arm clock as per above frequencies? Any issues if configured to be slower or faster than the frequencies above?

ラベル(1)
2 返答(返信)

2,332件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nigel

operation above max. frequency defined in datasheet is not guaranteed, for below

there are no restrictions. One can look at datasheets for particular part, for i.MX6UL

it is below link

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz |NXP 

Reliability is described in AN1598 i.MX 6UltraLite Product Usage Lifetime

https://www.nxp.com/docs/en/application-note/AN5198.pdf 

The same documents can be found on appropriate i.MX product pages.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,332件の閲覧回数
n_po
Contributor I

Thanks Igor!

0 件の賞賛
返信