Logcat crashes with error: unexpected EOF in Android 9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Logcat crashes with error: unexpected EOF in Android 9

Jump to solution
4,882 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on i.MX 6Quad SABRE-SD with Android 9. Logcat crashing after increment the buffer size also. I configured buffer size to 200Mb.

logcat -G 200Mb (before 64 Kb)

But, even though I got the EOF error. 

Is there any other configuration do we need to for increase buffer size automatically ?

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
Labels (2)
0 Kudos
Reply
1 Solution
4,548 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

This is caused by the lack of RAM memory in the sabreSD board. Unfortunately, a buffer of 200MB is a lot for the i.MX 6Quad SABRE-SD since the board only has 1 GB of RAM. I apologize for the inconvenience this could give you.

Best regards,

Diego.

View solution in original post

0 Kudos
Reply
2 Replies
4,549 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

This is caused by the lack of RAM memory in the sabreSD board. Unfortunately, a buffer of 200MB is a lot for the i.MX 6Quad SABRE-SD since the board only has 1 GB of RAM. I apologize for the inconvenience this could give you.

Best regards,

Diego.

0 Kudos
Reply
4,548 Views
vinothkumars
Senior Contributor IV

Thank you Diego,

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply