Linux ns-world

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux ns-world

1,690件の閲覧回数
ailtonlopes
Contributor III

Hi, im working with the Trustzone on the IMX6QSD board and i wanted to ask id there's a way to use linux as non-secure in the board.
Kind regards, 

Ailton Lopes

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,535件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   customers can try the recent NXP Linux BSP L4.9.88, which supports Optee, but it

is not enabled by default. For how to enable it, see ReadMe.

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Documentation - OP-TEE 

Regards,

Yuri.

0 件の賞賛
返信

1,535件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the topic as below, hope helpful for you

https://community.nxp.com/message/650147 

0 件の賞賛
返信