Adc values read from boot loader in IMx6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adc values read from boot loader in IMx6UL

1,251 次查看
sankarsalla
Contributor II

Hi All,

In my project need to read adc values from boot loader.

Adc values are read from root file system happens through sysfs entries and properly working.

Same thing i need to read from boot loader,i have checked in boot loader source adc driver is not there.

can you help me how to port adc driver in boot loader.

Thanks & Regards,

Sankar.      

标签 (1)
0 项奖励
回复
1 回复

1,174 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sankar

for baremetal adc examples one can look at freertos:

Board Support Packages (7)
SDK2.2_iMX6UL_WIN(REV SDK2.2)

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz |NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复