Linux hangs in Non-secure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux hangs in Non-secure

1,437 Views
ailtonlopes
Contributor III

Hi, im trying to run linux on the imx6q  SD board and the kernel runs fine when running as secure and when i switch to non secure the kernel hags. I believe that the problem is that the kernel is trying to access some peripheral that doesn't allow non-secure access and it's causing the crash but don't know which one. 

Here is the kernel output.

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.15.0 (andersen@andersenbond) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.18
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] cma: Reserved 64 MiB at 0x4c000000
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at arch/arm/kernel/devtree.c:157 arm_dt_init_cpu_maps+0x108/0x170
[ 0.000000] DT /cpu 2 nodes greater than max cores 1, capping them
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 4.15.0 #26
[ 0.000000] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 0.000000] Backtrace:
[ 0.000000] [<c01068f8>] (dump_backtrace) from [<c0106bc4>] (show_stack+0x18/0x1c)
[ 0.000000] r7:00000009 r6:00000000 r5:c0713448 r4:c0a01f00
[ 0.000000] [<c0106bac>] (show_stack) from [<c054599c>] (dump_stack+0x20/0x28)
[ 0.000000] [<c054597c>] (dump_stack) from [<c011b034>] (__warn+0xd4/0xfc)
[ 0.000000] [<c011af60>] (__warn) from [<c011b098>] (warn_slowpath_fmt+0x3c/0x44)
[ 0.000000] r8:eb9d694c r7:c0718c80 r6:c0713418 r5:00000001 r4:c0713464
[ 0.000000] [<c011b060>] (warn_slowpath_fmt) from [<c0804c3c>] (arm_dt_init_cpu_maps+0x108/0x170)
[ 0.000000] r3:00000002 r2:c0713464
[ 0.000000] r4:00000000
[ 0.000000] [<c0804b34>] (arm_dt_init_cpu_maps) from [<c080414c>] (setup_arch+0x7b8/0xa88)
[ 0.000000] r9:c118e230 r8:c0a1fe68 r7:4fffffff r6:ebffff40 r5:c0a09fe8 r4:c084605c
[ 0.000000] [<c0803994>] (setup_arch) from [<c08009f8>] (start_kernel+0x60/0x40c)
[ 0.000000] r10:10c53c7d r9:412fc09a r8:22000000 r7:c0a07080 r6:10c03c7d r5:00000051
[ 0.000000] r4:c080032c
[ 0.000000] [<c0800998>] (start_kernel) from [<00000000>] ( (null))
[ 0.000000] r10:10c53c7d r9:412fc09a r8:22000000 r7:00000f8c r6:10c03c7d r5:00000051
[ 0.000000] r4:c080032c
[ 0.000000] random: get_random_bytes called from print_oops_end_marker+0x40/0x50 with crng_init=0
[ 0.000000] ---[ end trace 0000000000000000 ]---
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 195072
[ 0.000000] Kernel command line: init=/init console=ttymxc0,115200
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 696588K/786432K available (5120K kernel code, 236K rwdata, 1700K rodata, 2048K init, 75)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (6112 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 237 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) (7577 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Running RCU self tests
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000010] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.000040] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.002049] Console: colour dummy device 80x30
[ 0.002084] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.002101] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.002116] ... MAX_LOCK_DEPTH: 48
[ 0.002130] ... MAX_LOCKDEP_KEYS: 8191
[ 0.002144] ... CLASSHASH_SIZE: 4096
[ 0.002156] ... MAX_LOCKDEP_ENTRIES: 32768
[ 0.002170] ... MAX_LOCKDEP_CHAINS: 65536
[ 0.002181] ... CHAINHASH_SIZE: 32768
[ 0.002195] memory used by lock dependency info: 4655 kB
[ 0.002208] per task-struct memory footprint: 1536 bytes
[ 0.002264] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=3)
[ 0.002301] pid_max: default: 32768 minimum: 301
[ 0.002589] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.002634] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.004923] CPU: Testing write buffer coherency: ok
[ 0.007925] Setting up static identity map for 0x20100000 - 0x20100078
[ 0.011067] devtmpfs: initialized
[ 0.047417] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.047478] futex hash table entries: 256 (order: 1, 11264 bytes)
[ 0.052091] pinctrl core: initialized pinctrl subsystem
[ 0.054265] NET: Registered protocol family 16
[ 0.074403] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.077615] cpuidle: using governor menu
[ 0.077795] CPU identified as i.MX6Q, silicon rev 1.2
[ 0.130173] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.130205] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.133628] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.190120] vgaarb: loaded
[ 0.191247] SCSI subsystem initialized
[ 0.194129] i2c i2c-0: IMX I2C adapter registered
[ 0.194174] i2c i2c-0: can't use DMA, using PIO instead.
[ 0.196330] i2c i2c-1: IMX I2C adapter registered
[ 0.196375] i2c i2c-1: can't use DMA, using PIO instead.
[ 0.197988] i2c i2c-2: IMX I2C adapter registered
[ 0.198032] i2c i2c-2: can't use DMA, using PIO instead.
[ 0.200863] clocksource: Switched to clocksource mxc_timer1
[ 0.201680] VFS: Disk quotas dquot_6.6.0
[ 0.201804] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.517427] hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
[ 0.517676] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 0.522470] Initialise system trusted keyrings
[ 0.523095] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[ 0.539176] fuse init (API version 7.26)
[ 0.543167] random: fast init done
[ 0.555892] Key type asymmetric registered
[ 0.556001] Asymmetric key parser 'x509' registered
[ 0.556142] io scheduler noop registered
[ 0.556172] io scheduler deadline registered
[ 0.556577] io scheduler cfq registered (default)
[ 0.556607] io scheduler mq-deadline registered
[ 0.556627] io scheduler kyber registered
[ 0.559875] OF: PCI: host bridge /soc/pcie@1ffc000 ranges:
[ 0.559955] OF: PCI: IO 0x01f80000..0x01f8ffff -> 0x00000000
[ 0.560095] OF: PCI: MEM 0x01000000..0x01efffff -> 0x01000000
[ 1.681567] imx6q-pcie 1ffc000.pcie: phy link never came up
[ 1.685351] imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00
[ 1.685398] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.685432] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.685460] pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
[ 1.686944] PCI: bus0: Fast back to back transfers disabled
[ 1.687330] PCI: bus1: Fast back to back transfers enabled
[ 1.687425] pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
[ 1.687468] pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]
[ 1.687496] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.688709] pcieport 0000:00:00.0: Signaling PME with IRQ 302
[ 1.689438] pcieport 0000:00:00.0: AER enabled with IRQ 302
[ 1.695907] imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
[ 1.696594] imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
[ 1.699287] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX
[ 2.446039] console [ttymxc0] enabled
[ 2.466438] etnaviv gpu-subsystem: bound 134000.gpu (ops gpu_ops)
[ 2.472782] etnaviv gpu-subsystem: bound 130000.gpu (ops gpu_ops)
[ 2.478984] etnaviv gpu-subsystem: bound 2204000.gpu (ops gpu_ops)
[ 2.485269] etnaviv-gpu 134000.gpu: model: GC320, revision: 5007
[ 2.520413] etnaviv-gpu 130000.gpu: model: GC2000, revision: 5108
[ 2.556070] etnaviv-gpu 2204000.gpu: model: GC355, revision: 1215
[ 2.562288] etnaviv-gpu 2204000.gpu: Ignoring GPU with VG and FE2.0
[ 2.571393] [drm] Initialized etnaviv 1.1.0 20151214 for gpu-subsystem on minor 0
[ 2.580833] ------------[ cut here ]------------
[ 2.585591] WARNING: CPU: 0 PID: 1 at ./include/linux/reset.h:67 ipu_probe+0x1cc/0x274
[ 2.593592] Modules linked in:
[ 2.596691] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.15.0 #26
[ 2.603900] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 2.610451] Backtrace:
[ 2.613000] [<c01068f8>] (dump_backtrace) from [<c0106bc4>] (show_stack+0x18/0x1c)
[ 2.620598] r7:00000009 r6:00000000 r5:c0749538 r4:00000000
[ 2.626346] [<c0106bac>] (show_stack) from [<c054599c>] (dump_stack+0x20/0x28)
[ 2.633659] [<c054597c>] (dump_stack) from [<c011b034>] (__warn+0xd4/0xfc)
[ 2.640568] [<c011af60>] (__warn) from [<c011b12c>] (warn_slowpath_null+0x44/0x50)
[ 2.648215] r8:eb9d3a78 r7:e82e8b40 r6:c045bf38 r5:00000043 r4:c0749538
[ 2.655001] [<c011b0e8>] (warn_slowpath_null) from [<c045bf38>] (ipu_probe+0x1cc/0x274)
[ 2.663085] r6:00000000 r5:e8140810 r4:e8267c10
[ 2.667745] [<c045bd6c>] (ipu_probe) from [<c046c0b0>] (platform_drv_probe+0x58/0xb4)
[ 2.675696] r10:00000000 r9:00000000 r8:c0a312ec r7:fffffdfb r6:c0a312ec r5:fffffffe
[ 2.683630] r4:e8140810
[ 2.686206] [<c046c058>] (platform_drv_probe) from [<c046a5a8>] (driver_probe_device+0x254/0x338)
[ 2.695158] r7:00000000 r6:c119e8ec r5:c119e8e8 r4:e8140810
[ 2.700854] [<c046a354>] (driver_probe_device) from [<c046a740>] (__driver_attach+0xb4/0xb8)
[ 2.709377] r10:c0a31ba8 r9:c046c058 r8:c046c010 r7:00000000 r6:e8140844 r5:c0a312ec
[ 2.717279] r4:e8140810 r3:00000000
[ 2.721126] [<c046a68c>] (__driver_attach) from [<c046888c>] (bus_for_each_dev+0x54/0xa4)
[ 2.729339] r7:00000000 r6:c046a68c r5:c0a312ec r4:00000000
[ 2.735097] [<c0468838>] (bus_for_each_dev) from [<c0469f08>] (driver_attach+0x20/0x28)
[ 2.743185] r6:c0a31ba8 r5:e82e3500 r4:c0a312ec
[ 2.747840] [<c0469ee8>] (driver_attach) from [<c04699e8>] (bus_add_driver+0x178/0x20c)
[ 2.755930] [<c0469870>] (bus_add_driver) from [<c046b0bc>] (driver_register+0x80/0xfc)
[ 2.764150] r7:c064e454 r6:00000000 r5:00000003 r4:c0a312ec
[ 2.769857] [<c046b03c>] (driver_register) from [<c046c1b4>] (__platform_register_drivers+0x5c/0xe4)
[ 2.779239] r5:00000003 r4:00000002
[ 2.782925] [<c046c158>] (__platform_register_drivers) from [<c083aa9c>] (imx_ipu_init+0x1c/0x24)
[ 2.791886] r10:c0800608 r9:c0847858 r8:00000007 r7:c07a7c70 r6:ffffe000 r5:c083aa80
[ 2.799741] r4:00000000
[ 2.802358] [<c083aa80>] (imx_ipu_init) from [<c0101adc>] (do_one_initcall+0x44/0x174)
[ 2.810316] [<c0101a98>] (do_one_initcall) from [<c0800eb8>] (kernel_init_freeable+0x114/0x1d0)
[ 2.819097] r8:00000007 r7:c07a7c70 r6:c0847850 r5:c08539fc r4:c0a3b240
[ 2.825890] [<c0800da4>] (kernel_init_freeable) from [<c0558974>] (kernel_init+0x10/0x114)
[ 2.834241] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0558964
[ 2.842145] r4:00000000
[ 2.844717] [<c0558964>] (kernel_init) from [<c01028d4>] (ret_from_fork+0x14/0x20)
[ 2.852362] r5:c0558964 r4:00000000
[ 2.855977] ---[ end trace 34f87c9ff0f06f1e ]---
[ 2.860627] imx-ipuv3 2400000.ipu: failed to reset: -524
[ 2.866106] imx-ipuv3: probe of 2400000.ipu failed with error -524
[ 2.872770] ------------[ cut here ]------------
[ 2.877438] WARNING: CPU: 0 PID: 1 at ./include/linux/reset.h:67 ipu_probe+0x1cc/0x274
[ 2.885449] Modules linked in:
[ 2.888551] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.15.0 #26
[ 2.895762] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 2.902360] Backtrace:
[ 2.904862] [<c01068f8>] (dump_backtrace) from [<c0106bc4>] (show_stack+0x18/0x1c)
[ 2.912515] r7:00000009 r6:00000000 r5:c0749538 r4:00000000
[ 2.918213] [<c0106bac>] (show_stack) from [<c054599c>] (dump_stack+0x20/0x28)
[ 2.925522] [<c054597c>] (dump_stack) from [<c011b034>] (__warn+0xd4/0xfc)
[ 2.932483] [<c011af60>] (__warn) from [<c011b12c>] (warn_slowpath_null+0x44/0x50)
[ 2.940085] r8:eb9d55ec r7:e82e8bc0 r6:c045bf38 r5:00000043 r4:c0749538
[ 2.946870] [<c011b0e8>] (warn_slowpath_null) from [<c045bf38>] (ipu_probe+0x1cc/0x274)
[ 2.954955] r6:00000000 r5:e8141810 r4:e8267c10
[ 2.959615] [<c045bd6c>] (ipu_probe) from [<c046c0b0>] (platform_drv_probe+0x58/0xb4)
[ 2.967531] r10:00000000 r9:00000000 r8:c0a312ec r7:fffffdfb r6:c0a312ec r5:fffffffe
[ 2.975436] r4:e8141810
[ 2.978006] [<c046c058>] (platform_drv_probe) from [<c046a5a8>] (driver_probe_device+0x254/0x338)
[ 2.986957] r7:00000000 r6:c119e8ec r5:c119e8e8 r4:e8141810
[ 2.992701] [<c046a354>] (driver_probe_device) from [<c046a740>] (__driver_attach+0xb4/0xb8)
[ 3.001223] r10:c0a31ba8 r9:c046c058 r8:c046c010 r7:00000000 r6:e8141844 r5:c0a312ec
[ 3.009077] r4:e8141810 r3:00000000
[ 3.012733] [<c046a68c>] (__driver_attach) from [<c046888c>] (bus_for_each_dev+0x54/0xa4)
[ 3.020989] r7:00000000 r6:c046a68c r5:c0a312ec r4:00000000
[ 3.026684] [<c0468838>] (bus_for_each_dev) from [<c0469f08>] (driver_attach+0x20/0x28)
[ 3.034764] r6:c0a31ba8 r5:e82e3500 r4:c0a312ec
[ 3.039419] [<c0469ee8>] (driver_attach) from [<c04699e8>] (bus_add_driver+0x178/0x20c)
[ 3.047507] [<c0469870>] (bus_add_driver) from [<c046b0bc>] (driver_register+0x80/0xfc)
[ 3.055590] r7:c064e454 r6:00000000 r5:00000003 r4:c0a312ec
[ 3.061334] [<c046b03c>] (driver_register) from [<c046c1b4>] (__platform_register_drivers+0x5c/0xe4)
[ 3.070491] r5:00000003 r4:00000002
[ 3.074152] [<c046c158>] (__platform_register_drivers) from [<c083aa9c>] (imx_ipu_init+0x1c/0x24)
[ 3.083104] r10:c0800608 r9:c0847858 r8:00000007 r7:c07a7c70 r6:ffffe000 r5:c083aa80
[ 3.091006] r4:00000000
[ 3.093575] [<c083aa80>] (imx_ipu_init) from [<c0101adc>] (do_one_initcall+0x44/0x174)
[ 3.101584] [<c0101a98>] (do_one_initcall) from [<c0800eb8>] (kernel_init_freeable+0x114/0x1d0)
[ 3.110313] r8:00000007 r7:c07a7c70 r6:c0847850 r5:c08539fc r4:c0a3b240
[ 3.117104] [<c0800da4>] (kernel_init_freeable) from [<c0558974>] (kernel_init+0x10/0x114)
[ 3.125452] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0558964
[ 3.133354] r4:00000000
[ 3.135923] [<c0558964>] (kernel_init) from [<c01028d4>] (ret_from_fork+0x14/0x20)
[ 3.143566] r5:c0558964 r4:00000000
[ 3.147170] ---[ end trace 34f87c9ff0f06f1f ]---
[ 3.151866] imx-ipuv3 2800000.ipu: failed to reset: -524
[ 3.157292] imx-ipuv3: probe of 2800000.ipu failed with error -524
[ 3.195224] brd: module loaded
[ 3.225696] loop: module loaded
[ 3.231137] i2c /dev entries driver
[ 3.241801] Loading compiled-in X.509 certificates
[ 3.310325] input: gpio-keys as /devices/soc0/gpio-keys/input/input0
[ 3.325334] Freeing unused kernel memory: 2048K
[ 3.337108] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004
[ 3.337108]
[ 3.346386] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004
[ 3.346386]  

Labels (2)
0 Kudos
Reply
1 Reply

1,168 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ailton

security accesses are managed by CSU module described in i.MX6DQ/SDL Security

Reference Manual available on

Q&amp;A: How is mx6 PMIC_ON_REQ under SW control? 

Seems one can debug it to find which module access causing panic using

AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply