_HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFC
PowerPrep start initialize power...
Battery Voltage = 1.88V
No battery or bad batterydetected!!!.Disabling batteryvoltage measurements./r/nLLCAug 22 201215:25:39
EMI_CTRL 0x1C084040
FRAC 0x92926192
init_ddr_mt46v32m16_133Mhz
power 0x00820710
Frac 0x92926192
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFCL0x80501001
on every power on above message dispalyed on RS232 debud port.
I am unable to find out hardware problem in my board. Any boby help me to boot the linux on my customize board.
Regards,
Pramod Kumar
DCP is responsible for Memory Copy. Next steep in your startup sequence should be uncompressing the kernel to your memory. Do you checked your memory?
You may change the imx-bootlets to activate (and extend) the memory test in the init-imx23.c bootlet source.
Dear Vasut,
Please guide me, how to check bootrpm reading the image from SD Card.
 
Boot image is O, it is working on i.Mx233 evk.
It seems some Hardware problem. Because board is designed by my self.
Regards,
Pramod Kumar
Check if the bootrom can read the image from your boot device correctly.
ROM ERROR CODE 0x80501001 means DCP reported a status error.
Looks like the boot image was not correctly prepared.
Please look at section 35.4 (General Boot Procedure) of i.MX233 Reference
Manual.