Linux booting halts after CAAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux booting halts after CAAM

1,528 Views
rendy
NXP Employee
NXP Employee

Hi,

 

We are working with i.MX 6SX and DS-5. We are connecting M4 core on Sabre board with uLink and DStream. In both cases the Linux booting halts after dumping of some CAAM keys. How can we prevent this? Or how to turn off CAAM in kernel config?

 

Thanks

Rene Kolarik

Original Attachment has been moved to: boot.log.zip

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,196 Views
Yuri
NXP Employee
NXP Employee

  Please look at my comments below.

1. 

  According to section 52.18 (Release a Slot back to the Keystore) of

“i.MX_6_Linux_Reference_Manual.pdf” ” in documentation of L3.14.28 :

“Configuration of the Secure Memory Driver / Keystore API is dependent on the

following kernel configuration parameters:

CRYPTO_DEV_FSL_CAAM_SM


Turns on the secure memory driver in the kernel build.

CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE

Configures the size of a secure memory "slot".

…

CRYPTO_DEV_FSL_CAAM_SM_TEST

Enables operation of a captive test / example module”

You may try to disable CAAM SM TEST.

“i.MX 6 Series Software and Development Tool Resources”

< http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW >

2.

  From Table 20 (Known issues and workarounds for i.MX 6SoloX) of
“i.MX_Linux_Release_Notes.pdf :

“The system reboots after the CAAM RNG test is suspended and resumed.
There is hardware function conflict between the Mega/Fast mix off feature and CAAM.
To use CAAM after kernel bootup, the user should enable the CAAM wakeup function
to avoid Mega mix off in DSM.
Workaround:
echo enabled > /sys/bus/platform/devices/2100000.aips-bus/2100000.caam/2101000.jr0/

  power/wakeup ”


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply