imx287 - freertos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx287 - freertos

2,759件の閲覧回数
ask
Contributor III

Hi,

Does anyone have a FreeRTOS port for imx287

Thanks for your time

0 件の賞賛
返信
3 返答(返信)

2,375件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you refer to the “Software and Tools” tab of i.MX287 webpage, you can find some RTOS options like MQX, Nucleus and QNX; however, FreeRTOS is not available.

According with FreeRTOS webpage, i.MX28 is not listed on the Freescale supported devices; however, the RTOS for ARM9 could be adapted for the i.MX287.

There are other options for the migration, like third parties services (here is an example):


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,375件の閲覧回数
TomE
Specialist II

This is the Coldfire Forum for MCFxxx parts. See if you can move your question to the i.MX forum:

i.MX Community

There should be a button or drop-down or something hidden somewhere that lets you move a post.

If you can find the "how do I use this forum forum" (used to be completely hidden) there may be an answer to that question there. That forum is here:

https://community.freescale.com/community/about

Tom

0 件の賞賛
返信

2,375件の閲覧回数
admin
Specialist II

Thanks Tom, I have moved the question to the i.MX Community

@ask please consider this general advice Where to post a Discussion? for better visibility.

Thank you for your interest in Freescale Community!

Denisse

0 件の賞賛
返信