Linux booting halts after CAAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux booting halts after CAAM

1,527件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

 

We are working with i.MX 6SX and DS-5. We are connecting M4 core on Sabre board with uLink and DStream. In both cases the Linux booting halts after dumping of some CAAM keys. How can we prevent this? Or how to turn off CAAM in kernel config?

 

Thanks

Rene Kolarik

Original Attachment has been moved to: boot.log.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,195件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please look at my comments below.

1. 

  According to section 52.18 (Release a Slot back to the Keystore) of

“i.MX_6_Linux_Reference_Manual.pdf” ” in documentation of L3.14.28 :

“Configuration of the Secure Memory Driver / Keystore API is dependent on the

following kernel configuration parameters:

CRYPTO_DEV_FSL_CAAM_SM


Turns on the secure memory driver in the kernel build.

CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE

Configures the size of a secure memory "slot".

…

CRYPTO_DEV_FSL_CAAM_SM_TEST

Enables operation of a captive test / example module”

You may try to disable CAAM SM TEST.

“i.MX 6 Series Software and Development Tool Resources”

< http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW >

2.

  From Table 20 (Known issues and workarounds for i.MX 6SoloX) of
“i.MX_Linux_Release_Notes.pdf :

“The system reboots after the CAAM RNG test is suspended and resumed.
There is hardware function conflict between the Mega/Fast mix off feature and CAAM.
To use CAAM after kernel bootup, the user should enable the CAAM wakeup function
to avoid Mega mix off in DSM.
Workaround:
echo enabled > /sys/bus/platform/devices/2100000.aips-bus/2100000.caam/2101000.jr0/

  power/wakeup ”


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信