Linux Test Project for i.MX6UL Linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Test Project for i.MX6UL Linux BSP

ソリューションへジャンプ
2,374件の閲覧回数
yuuki
Senior Contributor II

Dear all,

I have a question about LinuxBSP for i.MX6UL.

L3.14.38_iMX6UL (REV L3.14.38_6ul) is released as BSP for i.MX6UL.

Did an LTP test be executed on this BSP?

If there is the result of the LTP test, would you send it to me?

Best Regards,
Yuuki

ラベル(1)
0 件の賞賛
返信
1 解決策
2,084件の閲覧回数
b36401
NXP Employee
NXP Employee

Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.

Sorry for the inconvenience.

The package ltp-imx was used for early i.MX series, such as i.MX35,51.

Then it was replaced with OBDS - i.MX50,53,28.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,085件の閲覧回数
b36401
NXP Employee
NXP Employee

Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.

Sorry for the inconvenience.

The package ltp-imx was used for early i.MX series, such as i.MX35,51.

Then it was replaced with OBDS - i.MX50,53,28.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信