Linux Test Project for i.MX6UL Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Test Project for i.MX6UL Linux BSP

Jump to solution
2,370 Views
yuuki
Senior Contributor II

Dear all,

I have a question about LinuxBSP for i.MX6UL.

L3.14.38_iMX6UL (REV L3.14.38_6ul) is released as BSP for i.MX6UL.

Did an LTP test be executed on this BSP?

If there is the result of the LTP test, would you send it to me?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
2,080 Views
b36401
NXP Employee
NXP Employee

Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.

Sorry for the inconvenience.

The package ltp-imx was used for early i.MX series, such as i.MX35,51.

Then it was replaced with OBDS - i.MX50,53,28.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,081 Views
b36401
NXP Employee
NXP Employee

Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.

Sorry for the inconvenience.

The package ltp-imx was used for early i.MX series, such as i.MX35,51.

Then it was replaced with OBDS - i.MX50,53,28.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply