Linux Kernel 4.x for iMX251

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Kernel 4.x for iMX251

1,528件の閲覧回数
kevin11
Contributor I

Hi,

I am using Linux 2.6.31 on my platform, which is iMX251 3-stack board.

Wondering to know that is there anyone try to port Linux 4.x to this board and is willing to share your experience ?

The latest kernel and BSP release on linux-imx.git is version 4.9.11_1.0.0_ga.

Would it be OK to start porting based on this version ?

Regards,

Kevin

ラベル(2)
0 件の賞賛
返信
1 返信

1,357件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you want to port imx25 to yocto, right

I got information :

"

You need to prepare a patch for adding mx25pdk support into meta-fsl-arm.

 

Here is an example on how to add a new board:

http://patches.openembedded.org/patch/82199/

 

In this example Daiane added support for mx6 riotboard into meta-fsl-arm-extra. (The -extra means that this board is from third-party. The FSL boards go to meta-fsl-arm instead).

"

0 件の賞賛
返信