Linux BSP Build Instruction without Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux BSP Build Instruction without Yocto

1,907件の閲覧回数
JK-IMX
Contributor V

Hi NXP Champs.

Can anyone please give instruction to build Linux BSP especially for Uboot and Kernel without Yocto Project build?

I ask this help since it takes too long to get my image which has the change from U-boot and Kernel side only. 

I want to test modified Uboot and Kernel only rather than Rootfilesystem without Yocto build setup. 

Regards, 

James

0 件の賞賛
返信
2 返答(返信)

1,901件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello James,

You can read the yocto user guide document:

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

 

Regards

0 件の賞賛
返信

1,882件の閲覧回数
JK-IMX
Contributor V

Hi 

Thanks for your reply.

I asked the build instruction without Yocto SDK setup.

It would be useful when Customer would like to use Build Root Root filesystem rather than Yocto. 

Regards, 

Jack

0 件の賞賛
返信