Linux BSP Build Instruction without Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux BSP Build Instruction without Yocto

1,904 Views
JK-IMX
Contributor V

Hi NXP Champs.

Can anyone please give instruction to build Linux BSP especially for Uboot and Kernel without Yocto Project build?

I ask this help since it takes too long to get my image which has the change from U-boot and Kernel side only. 

I want to test modified Uboot and Kernel only rather than Rootfilesystem without Yocto build setup. 

Regards, 

James

0 Kudos
Reply
2 Replies

1,898 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello James,

You can read the yocto user guide document:

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

 

Regards

0 Kudos
Reply

1,879 Views
JK-IMX
Contributor V

Hi 

Thanks for your reply.

I asked the build instruction without Yocto SDK setup.

It would be useful when Customer would like to use Build Root Root filesystem rather than Yocto. 

Regards, 

Jack

0 Kudos
Reply