Latest Uboot and Kernel Version Supported for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest Uboot and Kernel Version Supported for IMX6

4,620 Views
rajniks
Contributor I

I have a LTIB L3.0.35_4.1.0 installed on a Unbutu 12.04 Linux host and version of Uboot and Kernel supported are given below

linux-3.0.35

uboot-2009.08

I wanted to know if there is a updated version supported now and if yes how can get the sourcecode and relevant patch files to update my ltib as well.

Labels (4)
Tags (4)
0 Kudos
Reply
6 Replies

2,183 Views
rajniks
Contributor I

I have followed Yocto User manual and downloaded it on my computer but it needs lot of resources and I have not been to able to build the default u-boot itself. LTIB was comparatively much lighter. I have LTIB working installation. Just wanted to know if Freescale supports both or I need to move to Yocto.

As of now I have not been successful with Yocto.

0 Kudos
Reply

2,183 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Freescale has moved the Linux BSP to Yocto.

Linux 3.10.17

o   Source Code Download Steps Documentation and Demo Images

Documentation:

o   Linux 3.10.17 BSP & MM Bundle

Also, you can find the latest Kernel and u-boot in the git.

http://git.freescale.com/git/

Luis

0 Kudos
Reply

2,183 Views
shabeerbadarudh
Contributor IV

Hi Luis ,

I downloaded both the source code and documents. But i am doubting about the header files.. In the Linux reference manual the header file location is ' <Yocto_BuildDir>/linux/arch/arm/plat-mxc/include/mach'. But in the 'plat-mxc' folder is missing in linux BSP. Where is the header file location in 3.10.17.

Regards

Shabeer

0 Kudos
Reply

2,183 Views
tonyzheng
NXP Employee
NXP Employee

Hi,Shabeer

In 3.10.17, you can try to find it in arch/arm/mach-imx.

0 Kudos
Reply

2,183 Views
rajniks
Contributor I

Hi Luis,

I tried to download through the git as discussed the PDF document "Freescale_Yocto_Project_User's_Guide" but looks like my organization has blocked git access. Is there any workaround to set this up?

0 Kudos
Reply

2,183 Views
tonyzheng
NXP Employee
NXP Employee

Hello,

You can use proxy server to download it. it need that you consult your organization's IT service and ask for proxy server IP.

0 Kudos
Reply