LVDS output on i.MX535 using Kernel v3.x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS output on i.MX535 using Kernel v3.x

1,424 Views
Rooney
Contributor III

Has anybody got the LVDS output working on Kernel v3.x??

The mainline kernel does not include any code for the framebuffer and IPU.

LVDS is working on v2.6.35 (Freescale BSP) and the i.MX53 QSB. How to port the relevant code from the v2.6.35 kernel to v3.x? Which files are relevant?

Regards,

Rooney

Tags (1)
0 Kudos
Reply
4 Replies

1,288 Views
RobertSchwebel
Contributor IV

Rooney,

it depends on your requirements. Please send me a mail with the features you need, to info@pengutronix.de.


Regards,

Robert

0 Kudos
Reply

1,288 Views
Rooney
Contributor III

Hello Robert!

Me again... how much will the port for the i.MX535 cost?

0 Kudos
Reply

1,288 Views
Rooney
Contributor III

Hello Robert!


Would be great to get commercial help, but it is not for a commercial product, so I cannot spend any money on that.

I'll try to extract the sources from the older kernel and port it to the newer kernel. I'm afraid that it will be very time-consuming...

0 Kudos
Reply

1,288 Views
RobertSchwebel
Contributor IV

Rooney,

we have LVDS running, with mainline + the DRM/KMS drivers posted on ALKML recently, plus additional IPU drivers which are currently made ready for mainline. This is all currently being ported towards 3.5-rc, in order to get more of the components mainline. It is a complex task and we are sharing the effort between different customers.

If you need commercial help, please drop me a note.


Regards,

Robert

0 Kudos
Reply