LVDS output on i.MX535 using Kernel v3.x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS output on i.MX535 using Kernel v3.x

1,425件の閲覧回数
Rooney
Contributor III

Has anybody got the LVDS output working on Kernel v3.x??

The mainline kernel does not include any code for the framebuffer and IPU.

LVDS is working on v2.6.35 (Freescale BSP) and the i.MX53 QSB. How to port the relevant code from the v2.6.35 kernel to v3.x? Which files are relevant?

Regards,

Rooney

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,289件の閲覧回数
RobertSchwebel
Contributor IV

Rooney,

it depends on your requirements. Please send me a mail with the features you need, to info@pengutronix.de.


Regards,

Robert

0 件の賞賛
返信

1,289件の閲覧回数
Rooney
Contributor III

Hello Robert!

Me again... how much will the port for the i.MX535 cost?

0 件の賞賛
返信

1,289件の閲覧回数
Rooney
Contributor III

Hello Robert!


Would be great to get commercial help, but it is not for a commercial product, so I cannot spend any money on that.

I'll try to extract the sources from the older kernel and port it to the newer kernel. I'm afraid that it will be very time-consuming...

0 件の賞賛
返信

1,289件の閲覧回数
RobertSchwebel
Contributor IV

Rooney,

we have LVDS running, with mainline + the DRM/KMS drivers posted on ALKML recently, plus additional IPU drivers which are currently made ready for mainline. This is all currently being ported towards 3.5-rc, in order to get more of the components mainline. It is a complex task and we are sharing the effort between different customers.

If you need commercial help, please drop me a note.


Regards,

Robert

0 件の賞賛
返信