LVDS on IMX6 Linux split-mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS on IMX6 Linux split-mode

3,098 Views
cristiansicilia
Contributor III

I'm try to working with an APALIS from TORADEX (IMX6 quad) to work with an LVDS dual channel display 1920x1200, but I get this result:


This is the configuration for ldb:

&ldb {
 status = "okay";
 split-mode; /// <<< -- added this or it desen't work at all
// dual-mode;

 lvds-channel@0 {
 reg = <0>;
 fsl,data-mapping = "spwg"; /* "jeida"; */
 fsl,data-width = <18>;
 crtc = "ipu2-di1";
 primary;


I tried this two configuration for timing

First:
 timing_wuxga: 1920x1200 {
                                clock-frequency = <150000000>;
                                hactive = <1920>;
                                vactive = <1200>;
                                hback-porch = <50>;
                                hfront-porch = <50>;
                                vback-porch = <5>;
                                vfront-porch = <5>;
                                hsync-len = <38>;
                                vsync-len = <2>;
                                hsync-active = <0>;
                                vsync-active = <0>;
                                pixelclk-active = <0>;
                        };


Second:
                        timing_wuxga: 1920x1200 {
                                clock-frequency = <150000000>;
                                hactive = <1920>;
                                vactive = <1200>;
                                hback-porch = <60>;
                                hfront-porch = <60>;
                                vback-porch = <5>;
                                vfront-porch = <5>;
                                hsync-len = <18>;
                                vsync-len = <2>;
                                hsync-active = <0>;
                                vsync-active = <0>;
                                pixelclk-active = <0>;
                        };



Just now I'm trying this but I don't think change the result




                        timing_wuxga: 1920x1200 {
                                clock-frequency = <150000000>;
                                hactive = <1920>;
                                vactive = <1200>;
                                hback-porch = <69>;
                                hfront-porch = <69>;
                                vback-porch = <6>;
                                vfront-porch = <6>;
                                hsync-len = <0>;
                                vsync-len = <0>;
                                hsync-active = <0>;
                                vsync-active = <0>;
                                pixelclk-active = <0>;
                        };

‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍




Some information about the display

pastedImage_2.png

pastedImage_3.png

0 Kudos
Reply
1 Reply

2,937 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

toradex boards use own linux from linux-toradex.git and one can

check toradex resources on that subject:

LVDS clock setting IMX6 Apalis - Toradex Community 

Split mode LVDS to eDP via bridge - Toradex Community 

LVDS split mode vs. dual mode / IMX6 / EGLFS - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply