LTIN :: U-boot :: Modifications needed in the program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIN :: U-boot :: Modifications needed in the program

1,265件の閲覧回数
KrishnaPavan
Contributor II

CPU:   Freescale i.MX51 family 3.0V at 800 MHz
mx51 pll1: 800MHz
mx51 pll2: 665MHz
mx51 pll3: 216MHz
ipg clock     : 66500000Hz
ipg per clock : 665000000Hz
uart clock    : 54000000Hz
cspi clock    : 54000000Hz
axi_a clock   : 166250000Hz
axi_b clock   : 133000000Hz
emi_slow clock: 83125000Hz
ddr clock     : 166250000Hz
esdhc clock   : 216000000Hz
Board: MX51 BABBAGE 3.0 [POR]
Boot Device: MMC
I2C:   ready
DRAM:  512 MB
MMC:   FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment

In:    serial
Out:   serial
Err:   serial
PMIC Mode: SPI
Net:   got MAC address from IIM: 00:ab:cd:ef:gh:ij
FEC0 [PRIME]
Hit any key to stop autoboot:  0
*** ERROR: `serverip' not set
Wrong Image Format for bootm command
ERROR: can't get kernel image!
BBG U-Boot >

 

 

 

 

 

 

 

 

Working on Ubuntu 10.04

I have followed the exact procedure i.e.,given in the manual, for flashing but the problem is with the modifiaction of the deafult environment

The error lead me to the file

/home/user/ltib/u-boot 2009.08/common/env_nand.c

 

from which I understand that I need to modify the entry point in the ROM while flashing within the code, something  something etc.......

Can you help me get through this..

I have highlighted the eroors..... to bring them to your attention

regards./...............Krishna Pavan

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)