LTIB "Failed building wget" undefined reference to `SSLv2_client_method'
I was following the LTIB guide:
Ubuntu 11.10 Oneiric 64-bit Virtual Machine and building i.MX53 L2.6.35-11-09-01
I got past the zlib issues by following:
http://vijay496.blogspot.com/2012/03/ltib-for-ubuntu-1110-error-fac...
Now: I am having wget package failing.
I am running Ubuntu 11.10, 32-bit.
Anyone ever got the error below, thanks?
Ad.
-----------------
gcc -O2 -Wall -Wno-implicit -o wget cmpt.o connect.o convert.o cookies.o ftp.o ftp-basic.o ftp-ls.o ftp-opie.o hash.o headers.o host.o html-parse.o html-url.o http.o init.o log.o main.o gen-md5.o netrc.o progress.o rbuf.o recur.o res.o retr.o safe-ctype.o snprintf.o gen_sslfunc.o url.o utils.o version.o -lssl -lcrypto -ldl
gen_sslfunc.o: In function `init_ssl':
gen_sslfunc.c:(.text+0x351): undefined reference to `SSLv2_client_method'
collect2: ld returned 1 exit status
make[1]: *** [wget] Error 1
make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1/src'
make: *** [src] Error 2
error: Bad exit status from /home/me/imx53/11.09.01/ltib/tmp/rpm-tmp.33663 (%build)
RPM build errors:
Bad exit status from /home/me/imx53/11.09.01/ltib/tmp/rpm-tmp.33663 (%build)
Build time for wget: 21 seconds
Failed building wget
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
Started: Mon May 21 00:16:07 2012
Ended: Mon May 21 00:16:28 2012
Elapsed: 21 seconds
These packages failed to build:
wget
Build Failed
I am not sure what do you mean by having SSL installed? Do you have it installed on the LTIB platform or on your Ubuntu?
OpenSSL is a part of the LTIB distribution, so try compiling it from there for your iMX target and see if you get the wget error again.
Debian and Ubuntu openssl distro packages are built with -DOPENSSL_NO_SSL2, i.e. SSLv2 disabled. To enable, you need either to compile wget without SSL at all, or compile openssl from source yourself. Here are the directions to compile openssl yourself:
- Download openssl-1.0.1f.tar.gz from http://www.openssl.org/source/openssl-1.0.1f.tar.gz
- Open the OpenSSL tarball: yba@tavas:/usr/local/src# zcat openssl-1.0.1f.tar.gz | tar xvf -
- pushd openssl-1.0.1f/
- ./config shared
- make
- sudo make install
- In ltib installation directory do export LDFLAGS=-L/usr/local/ssl/lib; export CPPFLAGS=-I/usr/local/ssl/include
- ./ltib
Note that you might have to do rm -rf /opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1 if the wget build already failed.
This solution only worked if instead of step 7, I executed `export LDFLAGS=-L/usr/local/ssl/lib`
Ivica,
I tried both and only disabling SSL in the spec file worked.
I am worried some automated scripts that use wget will break if they try
to get from https sites :(
But that is a different issue.
Thanks,
Ad.
............
Do I need to compile OpenSSL maually or apt-get will do?
I do have openssl installed but I can't find any plain developer version
when I do l "sudo aptitude search openssl".
Thanks,
Ad.
-----------------------
Ivica Eftimovski said:
I think you have two choices here:
1. Disable SSL by adding “--without-ssl” to the configure line in the *.spec file.
2. Compile OpenSSL. I think this is the only external SSL library that wget works with.
I think you have two choices here:
1. Disable SSL by adding “--without-ssl” to the configure line in the *.spec file.
2. Compile OpenSSL. I think this is the only external SSL library that wget works with.
hi,
Already "--without-ssl" is there in wget.spec file and even I installed OpenSSL, it is giving same issue "Failed building wget-ssl ".
Help me in solving this issue.
Thanks and regards,
Siva Prakash Reddy N
Hi,