LTIB_configure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB_configure

1,530 Views
meandyoursame
Contributor I

./ltib -m config error:

making filesystem image file
staging directory is /home/work/ltib_source/ltib/rootfs.tmp
find: `./opt/syslog': Permission denied
find: `./opt/historycali': Permission denied
removing the boot directory and files
removing man files and directories
removing info files
removing /usr/share/locale directory
removing /usr/man directory
removing static libraries
removing target rpm database
stripping binaries and libraries

Filesystem stats, including padding:

    Total size            = 75024k
    Total number of files = 1748

sh: 21: mkfs.jffs2: not found
Died at ./ltib line 603, <> line 764.
traceback:
 main:603


Started: Wed Dec 14 18:28:44 2016
Ended:   Wed Dec 14 18:29:08 2016
Elapsed: 24 seconds


Build Failed

Exiting on error or interrupt

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,441 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please check that ltib was not installed as the super user to avoid issues

with access permissions. Refer to AN3875
http://www.nxp.com/assets/documents/data/en/application-notes/AN3875.pdf

Ltib on 11.10 host 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply