LTIB Image file size estimation and NAND Compression techniques.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LTIB Image file size estimation and NAND Compression techniques.

跳至解决方案
1,520 次查看
VikramU_ng
Contributor III

Dear Support,

   is there an estimate available on the actual root image file sizes when LTIB is built for a specific architecture. I understand the PDK comes with 2GB NAND. Is there a rough guide on the kernel and the rootfs filesizes in advance?.

net@net-PC:~/Qt_imx257/ltib/rootfs$ ls -lh root*


net@net-PC:~/Qt_imx257/ltib/rootfs$ cd ..
net@net-PC:~/Qt_imx257/ltib$ ls -lh root*
-rw-r--r--  1 net net  15M 2011-09-13 21:56 rootfs.cramfs
lrwxrwxrwx  1 net net   15 2011-09-13 21:56 rootfs_image -> ./rootfs.cramfs

 

Is the current filesize seen for the Image correct?. I have been unable to find resources to compress/compare various image formats. Could someone provide any specific document on this?.

 

 

regards,

Vikram U
标记 (1)
0 项奖励
回复
1 解答
1,393 次查看
VikramU_ng
Contributor III

A year later..

   i think the reliable guide is to identify the Base package - 300MB and then add the packages that need to go in.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,394 次查看
VikramU_ng
Contributor III

A year later..

   i think the reliable guide is to identify the Base package - 300MB and then add the packages that need to go in.

0 项奖励
回复