LTIB Build Failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB Build Failed

6,214 次查看
kolanchi
Fresh Out Contributor

Hi,

I facing problem while building gstreamer in LTIB environment. my LTIB version is L2.6.35_10.12.01_ER_source.
These are the version of my LTIB source.

1. gstreamer-0.10.25
2. gst-pluging-base-0.10.25
3.gst-plugins-good-0.10.16

So, I replaced these three plugin respectively gstreamer-0.10.32 , gst-plugins-base-0.10.32 , gst-plugins-good-0.10.28 my LTIB source.

After building LTIB source gstreamer-0.10.32 installed properly. while building gst-plugins-base-0.10.32 we are facing problem.

I replaced these three pkgs in /ltib/rpm/SOURCES/ this directory.

Guide me how to build the newer version gstreamer, base and good on LTIB environment.

Please refer the document for how to build the gstreamer in LTIB environment.

Below I am mentioning the error message.

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.4.4/../../../../arm-fsl-linux-gnueabi/bin/ld: warning: libgstvideo-0.10.so.0, needed by ../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so, not found (try using -rpath or -rpath-link)
../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_format_parse_caps'
../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_parse_caps_framerate'
../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_parse_caps_pixel_aspect_ratio'
../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_format_parse_caps_interlaced'
collect2: ld returned 1 exit status
make[4]: *** [encoding] Error 1
make[4]: Leaving directory `/home/kolanchi/VM/ltib/rpm/BUILD/gst-plugins-base-0.10.32/tests/examples/encoding'
make[3]: *** [encoding] Error 2
make[3]: Leaving directory `/home/kolanchi/VM/ltib/rpm/BUILD/gst-plugins-base-0.10.32/tests/examples'
make[2]

标签 (1)
标记 (2)
0 项奖励
回复
9 回复数

5,558 次查看
KrishnaPavan
Fresh Out Contributor

Hi,

According to the package, I think you need to attach this patch also according to the version, and place this patch in the pkgs directory.

Hope it works...

Regards  :: Krishna Pavan

0 项奖励
回复

5,558 次查看
albfon
Contributor II

Sorry to revive this old post, but today I found the same problem trying to update gstreamer from ltib (from 0.10.15 to 0.10.35).


I have patched sucesfully with the path above, but i have the same result,


../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_format_parse_caps'

../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_parse_caps_framerate'

../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_parse_caps_pixel_aspect_ratio'

../../../gst-libs/gst/pbutils/.libs/libgstpbutils-0.10.so: undefined reference to `gst_video_format_parse_caps_interlaced'

At the end could you do the update??

Thank you very much


0 项奖励
回复

5,558 次查看
kolanchi
Fresh Out Contributor

Hi Pavan,

                I have included below patch in my source as well as mention in the spec file also.

gst-plugins-base-0.10.22-mpeg2avsyncfix.patch
gst-plugins-base-0.10.22-typefindaacplus2flac.patch
gst-plugins-base-0.10.25-optplaybin2.patch
gst-plugins-base-0.10.25-optplaybin-v2.patch

Rgds,

kolanchi
Krishna Pavan said:

Hi, Some hassles listed  here!

0 项奖励
回复

5,558 次查看
KrishnaPavan
Fresh Out Contributor

Hi, Some hassles listed  here!

0 项奖励
回复

5,558 次查看
KrishnaPavan
Fresh Out Contributor

Hi Kolanchinathan,

o.k I have got the patch for it,

Include this patch in spec as well as in pkgs directory.

I dont think upgrading is this easy.  Lot many soname libraries are needed.

Regards :: Krishna Pavan

0 项奖励
回复

5,558 次查看
kolanchi
Fresh Out Contributor

Hi Pavan,

I have attached the spec file.

Rgds

kolanchi.

0 项奖励
回复

5,558 次查看
KrishnaPavan
Fresh Out Contributor

Hi Kolanchinathan,

Can you attach the spec file here?

0 项奖励
回复

5,558 次查看
kolanchi
Fresh Out Contributor

Hi Pavan,

              I modified the spec file based on my version. still I am facing the error.

Rgds,

kolanchi

Krishna Pavan said:

Hi,

Just catch the spec file in ltib directory and edit the specs with the required version.

Regards  ::    Krishna Pavan

0 项奖励
回复

5,558 次查看
KrishnaPavan
Fresh Out Contributor

Hi,

Just catch the spec file in ltib directory and edit the specs with the required version.

Regards  ::    Krishna Pavan

0 项奖励
回复