LTIB Build: Commad Prompt and Graphics interface is not coming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB Build: Commad Prompt and Graphics interface is not coming

1,994件の閲覧回数
Swamy
Fresh Out Contributor

Hello All,

 

I am building the image using LTIB for the first-time for IMX53. I was able to build it successfully after few hickups. But when I finally copied the image to sdcard(UImage, rootfs), i could not see the prompt or graphic interface. could you please tell me what all I am missing. I have attached the boot logs.

Thanks in advance

Regards,

Swamy

タグ(1)
0 件の賞賛
返信
1 返信

1,857件の閲覧回数
LuisCasado
NXP Employee
NXP Employee
Hello, What ltib profile are you building? Min, Gnome,.? What bsp version? Have a look to the BSP release notes of the BSP version tou are worwig with. Video commadnd line patameters have changed a little in the last BSPs. only Gnome mobile will init a graphic interface, Can you see Tux on the display at booting up? Best Regards,
0 件の賞賛
返信