LTIB Build: Commad Prompt and Graphics interface is not coming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB Build: Commad Prompt and Graphics interface is not coming

1,978 Views
Swamy
Contributor III

Hello All,

 

I am building the image using LTIB for the first-time for IMX53. I was able to build it successfully after few hickups. But when I finally copied the image to sdcard(UImage, rootfs), i could not see the prompt or graphic interface. could you please tell me what all I am missing. I have attached the boot logs.

Thanks in advance

Regards,

Swamy

Tags (1)
0 Kudos
Reply
1 Reply

1,841 Views
LuisCasado
NXP Employee
NXP Employee
Hello, What ltib profile are you building? Min, Gnome,.? What bsp version? Have a look to the BSP release notes of the BSP version tou are worwig with. Video commadnd line patameters have changed a little in the last BSPs. only Gnome mobile will init a graphic interface, Can you see Tux on the display at booting up? Best Regards,
0 Kudos
Reply