LSM6DSL Linux driver, Temperature sensor reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LSM6DSL Linux driver, Temperature sensor reading

ソリューションへジャンプ
2,330件の閲覧回数
_ZZ_
Contributor II

Hi,

Below is the Linux driver for lsm6dsl inertial module which has a temperature sensor in it. The driver doesn't seem to have any function or API to read the temperature sensor. Has anyone added the temperature reading to the driver ? 

https://elixir.bootlin.com/linux/latest/source/drivers/iio/imu/st_lsm6dsx

Thanks for any help,

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,307件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @_ZZ_,

I hope you are doing well.

Yes, the st_lsm6dsx driver has IIO channels for only the monitoring axis, it does not have any functionality to read the temperature.

One can contact sensor vendor regarding this issue,

Thanks & Regards,
Dhruvit Vasavada

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,308件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @_ZZ_,

I hope you are doing well.

Yes, the st_lsm6dsx driver has IIO channels for only the monitoring axis, it does not have any functionality to read the temperature.

One can contact sensor vendor regarding this issue,

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信