LS2088A processor highest Exception level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2088A processor highest Exception level

1,442 Views
vijaykumardesai
Contributor II

I am using LS2088ARDB board, U-boot leaves me in EL2.

So is it that ls2088a does not have EL3? or U-boot leaves in EL2?

I tries executing 'smc' instruction nothing happens.

   - If EL3 was implemented and I would assume it should have trapped

   - If EL3 was not implemented I expect it to my exception routine of EL2.

0 Kudos
Reply
1 Reply

1,359 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. This file is available in u-boot source code in NXP LSDK 1709.

See information about EL2 and EL3 in the u-boot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply